RTC off when no external oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC off when no external oscillator

1,932件の閲覧回数
carrielbr
Contributor II

Good Morning.

 

I am running RTC MK20DX256VLL10, however to turn off the chip and remove the oscillator 32Khz my RTC stops working. Its detect if the crystal was removed by the User when the chip is not powered (connected only with the RTC battery)?

 

Thank you

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,781件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Ciao,

Unfortunately, there is not such feature for RTC in K20, there is only a clock monitor that allows user to detect when RTC CLKOUT signal is lost (MCG_C8[CME1] bit), however, it does not apply when MCU is in low power modes or when MCU is not powered up. In other words, It can help you to detect if RTC CLK OUT signal is lost only when MCU is fully powered.

Regards,

Isaac

0 件の賞賛
返信