RTC off when no external oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC off when no external oscillator

2,022 Views
carrielbr
Contributor I

Good Morning.

 

I am running RTC MK20DX256VLL10, however to turn off the chip and remove the oscillator 32Khz my RTC stops working. Its detect if the crystal was removed by the User when the chip is not powered (connected only with the RTC battery)?

 

Thank you

Labels (1)
0 Kudos
Reply
1 Reply

1,871 Views
isaacavila
NXP Employee
NXP Employee

Hello Ciao,

Unfortunately, there is not such feature for RTC in K20, there is only a clock monitor that allows user to detect when RTC CLKOUT signal is lost (MCG_C8[CME1] bit), however, it does not apply when MCU is in low power modes or when MCU is not powered up. In other words, It can help you to detect if RTC CLK OUT signal is lost only when MCU is fully powered.

Regards,

Isaac

0 Kudos
Reply