Port of KL26Z to KSDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Port of KL26Z to KSDK

跳至解决方案
1,374 次查看
rshea
Contributor I

Checking in to see if anyone else has worked on creating a KL26Z port for the KSDK.

 

I am working on a project using both the KL26Z processor and the K22.  The KSDK is a good fit for the project and using the KSDK would make it easy to share common chunks of code between the two processors.  To this end I'm starting a KL26Z port for the KSDK targeting the drivers needed for my application.  If anyone else has already been down this path, I'd love a pointer to the code to save me from repeating the work.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,277 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Roy,

As I know, KSDK 1.1 will be available in the end of Dec.and KL03 and L4K will be supported in this release, maybe you can start your porting based on that version, or use KL03/L4K instead? BTW, 1.2GA will support KL26Z, and it will be available in Apr.2015.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,278 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Roy,

As I know, KSDK 1.1 will be available in the end of Dec.and KL03 and L4K will be supported in this release, maybe you can start your porting based on that version, or use KL03/L4K instead? BTW, 1.2GA will support KL26Z, and it will be available in Apr.2015.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,277 次查看
rshea
Contributor I

Thank you for the details on upcoming releases of the KSDK.  Great to know that support is coming down the line, so I'll keep my port to a bare bones minimum needed for our application.

0 项奖励
回复