No GPIO Peripheral Driver in KSDK 1.3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No GPIO Peripheral Driver in KSDK 1.3?

3,083 Views
audi_mcavoy
Contributor IV

I migrated a project from KSDK 1.2 to 1.3 and have a problem with my fsl_gpio component (in PEx).  After fighting with it for an hour or so, I decided to just delete the old component and add a new, fresh component.

 

Guess what.  There appears to be no fsl_gpio component available.  In fact, there appears to be a HUGE pile of components missing.

 

Here's a couple of screen shots to demonstrate. . .

 

KSDK 1.2.0 (note the fsl_gpio component near the bottom)

90539_90539.pngpastedImage_1.png

 

KSDK 1.3.0 (notice that this list starts at the fsl_gpio_hal component!)

90540_90540.pngpastedImage_2.png

 

There is a message at the bottom of these windows that says "Filtering disabled."

 

Are all of these components really missing?  Or is my install borked?

- Audi

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,821 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Audi,

Which chip do you use ? I check the k64 , it have the fsl_gpio component :

pastedImage_0.png

Hope it can help you !

Alice

0 Kudos
Reply

2,821 Views
audi_mcavoy
Contributor IV

I had filters turned off.  Even if I filter for the K64 processor, I still don't see many of the components I expect.

So what's the best thing for me to do?  Uninstall then reinstall KSDK 1.3?

Is it safe to just reinstall 1.3 on top of itself?

I do see the fsl_gpio_driver.c file in the ...\platform\driver\src\gpio\ folder.

Is there a better way to refresh KDS so it finds the missing components?

0 Kudos
Reply

2,821 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Audi,

What's the version of your KDS ? 

And i see the "fsl_gpio_hal" on your screenshot,  please check the place above  the "fsl_gpio_hal " ,

pastedImage_0.png

pastedImage_1.png

Hope it helps

Alice

0 Kudos
Reply

2,821 Views
audi_mcavoy
Contributor IV

Hi Alice,

Thanks for responding.

I'm using KDS 3.0.0.  Four days ago, there was no "place above fsl_gpio.hal" in my list.  That was the top of the list.

I reopened my project this morning, and guess what?  All of my KSDK 1.3.0 components decided to come out and play.

I see all of my components for both libraries.  The only thing I've done different since then is import and build the Kinetis flashloader project to start working with that.

I don't know what to say.  I'll just keep plodding forward until I trip over the next invisible twig in the path.

Thanks again.

- Audi

0 Kudos
Reply

2,821 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Audi,

OK,  in any case , you can develop you project  now ,:smileyhappy:

BR

Alice

0 Kudos
Reply