MMCAU in Keil uVision for K70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMCAU in Keil uVision for K70

Jump to solution
3,833 Views
yanivb
Contributor I

Dear NXP/community support,

I'm trying to operate the K70's MMCAU in uVision IDE (MQX RTOS).

I've downloaded the KSDK and got the MMCAU lib, but can't use these assembly files in uVision.

has anyone encountered this, or done this before ? 
I would appreciate any help,

Thanks in advance,

Yaniv

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
3,702 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Yaniv Bar on,

Thank you for your interest in the NXP kinetis product, I would like to provide service for you.
Do you mind to use the iar version?
Because I find one our application note contains the mmcau IAR project.
Maybe you also can refer to the IAR project to migirate to your MDK.
Please download the an4307 and it's software:
https://www.nxp.com/docs/en/application-note/AN4307.pdf
https://www.nxp.com/docs/en/application-note-software/AN4307SW.zip

Please check it on your side.
The code is based on the K60, but you can refer to it.

BTW, I find the TWRK-K60D100 sdk contains the mmcau MDK project, you can download it from this link:

https://mcuxpresso.nxp.com/en/select 

pastedImage_2.png

Wish it helps you!
If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
3,703 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Yaniv Bar on,

Thank you for your interest in the NXP kinetis product, I would like to provide service for you.
Do you mind to use the iar version?
Because I find one our application note contains the mmcau IAR project.
Maybe you also can refer to the IAR project to migirate to your MDK.
Please download the an4307 and it's software:
https://www.nxp.com/docs/en/application-note/AN4307.pdf
https://www.nxp.com/docs/en/application-note-software/AN4307SW.zip

Please check it on your side.
The code is based on the K60, but you can refer to it.

BTW, I find the TWRK-K60D100 sdk contains the mmcau MDK project, you can download it from this link:

https://mcuxpresso.nxp.com/en/select 

pastedImage_2.png

Wish it helps you!
If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,702 Views
yanivb
Contributor I

Hi,

Thanks a lot, I used the K60 example with some changes for my K70 and it works !!!

Best regards,

Yaniv

0 Kudos
Reply
3,702 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Yaniv Bar on

   Thanks very good to hear it works on your side.

   If your question is solved, please help me to mark the correct answer, just to close this case.

  If you have any question in the future, welcome to create the new case, thanks.

 

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you hav

0 Kudos
Reply