MK60DN512 Custom Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK60DN512 Custom Board

1,167件の閲覧回数
w2vy
Contributor V

I am looking to porting the board configuration for a Tower board to match a custom board.

 

When I check the TWR-K60D100 I see that it uses the MK60DN512VMD10 and my board uses the MK50DN512VLQ10.

 

I think I have gotten very lucky, just a different package but the same derivative of K60 because the different package basically results in different pin muxing.

 

Does that sound right?

 

If so then I should be able to use the MK60D10 device (under CMSIS)

 

I also see under boards/ the twrk60d100m, but I am not sure how these (board and device) both get tied together.

 

I see the <board_name>.peb file, but no mention of the MK60D10 in it either.

 

Maybe I am venturing where no man (should?) go...

 

Anyone succeed at porting an existing device to a custom board?

 

Tom

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)