MK60DN512 Custom Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60DN512 Custom Board

1,191 Views
w2vy
Contributor V

I am looking to porting the board configuration for a Tower board to match a custom board.

 

When I check the TWR-K60D100 I see that it uses the MK60DN512VMD10 and my board uses the MK50DN512VLQ10.

 

I think I have gotten very lucky, just a different package but the same derivative of K60 because the different package basically results in different pin muxing.

 

Does that sound right?

 

If so then I should be able to use the MK60D10 device (under CMSIS)

 

I also see under boards/ the twrk60d100m, but I am not sure how these (board and device) both get tied together.

 

I see the <board_name>.peb file, but no mention of the MK60D10 in it either.

 

Maybe I am venturing where no man (should?) go...

 

Anyone succeed at porting an existing device to a custom board?

 

Tom

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies