Latest data sheet for TWRK60D100M board required

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Latest data sheet for TWRK60D100M board required

2,060 Views
sunilvasudevan
Contributor I

I am using tower board TWRK60D100M with 700-27291 REVA board.When I checked the data sheet,the one which is existing is not matching with the case of jumper for example J19 jumper information is not present in the data sheet.I am trying to give the target power through Jtag after enabling the target voltage from Jtag side by giving Power on perm through Jtag commander tool.But it not detecting 5 volt on the target side which I doubt of not placing the corresponding jumper on the board.#twr-k60d100m

Tags (1)
0 Kudos
Reply
1 Reply

1,974 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi sunil,

You can get the schematics from here https://community.nxp.com/message/507023 

Regards,

Jing

0 Kudos
Reply