KV5 microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KV5 microcontroller

2,248 Views
plato
Contributor I

when the production? When the other KDS, KSD kit KES configuration tool for KV5?

Labels (1)
0 Kudos
Reply
3 Replies

2,049 Views
kenbarfield
Contributor I

Hi All,

It would be nice to get an update on the SDK release date for the KV5. Is it still expected in June 2016?

I can't find any source for this family.

There is a suggestion to start with code for some other KVx part. But this seems to be a drastic path.

Note, I was recently told the part will release in May 2016 if it passes some life test.

Also I was able to get both 100 and 144 pin samples.

Regards All,

Ken

0 Kudos
Reply

2,049 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Ken,

for current plan for each KSDK release please regularly check Introducing Kinetis SDK v2

At the moment KSDK v2.0 has not finished support for KVx family but in older versions KSDK is support for FRDM-KV31F, TWR-KV31F120M, TWR-KV10Z32, FRDM-KV10Z, TWR-KV11Z75M and their MCU.

Best Regards,

Iva

0 Kudos
Reply

2,049 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Federico,

KV series for KSDK and KDS is planned for Release 4 – Mid June, 2016.

KV5x family as well.

Kind Regards,

Iva

0 Kudos
Reply