SDK Project Generator Tool in Win 7 32-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK Project Generator Tool in Win 7 32-bit

1,337 Views
BillHoyt
Fresh Out Contributor


After downloading this:

     Kinetis SDK Project Generator Tool (REV 2)

and attempting to run the "Windows" version (KSDK_Project_Generator.exe) on Windows 7 (32-bit) PC, this error occurs:

"The version of this file is not compatible with the version of Windows you're running.  Check your computer's system information to see whether you need an x86 (32-bit) or x64 (64-bit) version of the program, and then contact the software publisher"

My guess is this app is only for 64-bit Windows.

Labels (1)
0 Kudos
Reply
1 Reply

1,215 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Bill,

thank you for pointing out this!

Unfortunately I can confirm this issue also on my side.

I reported the bug, http://sw-jira.freescale.net/browse/PGKSDK-258

I will keep you informed about this.

Thank you.

Best Regards,

Iva

0 Kudos
Reply