KSDKv2 - New Device Support Announcement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDKv2 - New Device Support Announcement

1,040件の閲覧回数
mnorman
NXP Employee
NXP Employee

The next wave of device support in Kinetis SDK 2.0 (KSDKv2) is now available on http://kex.nxp.com web page. Click the Build an SDK to customize the SDK based on your configuration.

 

Boards:

FRDM-KL02Z 

FRDM-KL03Z 

FRDM-KL25Z 

FRDM-KL26Z 

FRDM-KL46Z 

FRDM-KL82Z 

TWR-K21D50M

TWR-K24F120M

TWR-K60D100M

TWR-KL25Z48M

TWR-KL82Z72M

TWR-KM34Z75M

Devices:

MK10DX128xxx10, MK10DX256xxx10, MK10DN512xxx10

MK11DX128Axxx5, MK11DX256Axxx5, MK11DN512Axxx5

MK11DX128xxx5, MK11DX256xxx5, MK11DN512xxx5

MK12DX128xxx5, MK12DX256xxx5, MK12DN512xxx5

MK20DX128xxx10, MK20DX256xxx10, MK20DN512xxx10

MK21DX128Axxx5, MK21DX256Axxx5, MK21DN512Axxx5

MK21DX128xxx5, MK21DX256xxx5, MK21DN512xxx5

MK22DX128xxx5, MK22DX256xxx5, MK22DN512xxx5

MK24FN256xxx12

MK30DX128xxx10, MK30DX256xxx10, MK30DN512xxx10

MK40DX128xxx10, MK40DX256xxx10, MK40DN512xxx10

MK50DX256xxx10, MK50DN512xxx10

MK51DX256xxx10, MK51DN256xxx10, MK51DN512xxx10

MK52DN512xxx10

MK53DX256xxx10, MK53DN512xxx10

MK60DX256xxx10, MK60DN256xxx10, MK60DN512xxx10

MKL02Z8xxx4, MKL02Z16xxx4, MKL02Z32xxx4

MKL03Z8xxx4, MKL03Z16xxx4, MKL03Z32xxx4

MKL14Z32xxx4, MKL14Z64xxx4

MKL15Z32xxx4, MKL15Z64xxx4, MKL15Z128xxx4

MKL16Z32xxx4, MKL16Z64xxx4, MKL16Z128xxx4, MKL16Z256xxx4

MKL24Z32xxx4, MKL24Z64xxx4, MKL25Z128xxx4

MKL25Z32xxx4, MKL25Z64xxx4, MKL26Z128xxx4

MKL26Z32xxx4, MKL26Z64xxx4, MKL26Z256xxx4

MKL34Z64xxx4

MKL36Z64xxx4, MKL36Z128xxx4, MKL36Z256xxx4

MKL46Z128xxx4, MKL46Z256xxx4

MKL82Z128xxx7

MKM34Z256xxx7

 

Release overview:

The Kinetis SDK is intended for use with Kinetis MCU product family based on the ARM Cortex-M series architectures. The release consists of:

  • Kinetis device support
    • Kinetis board support
    • Demo applications and examples
    • Middleware
      • § USB Stack
      • § TCP/IP stack
      • § File System
      • § RTOS
      • § CMSIS
      • Documentation
        • § Kinetis SDK v.2.0.0 Release Notes
        • § Kinetis SDK v.2.0 API Reference Manual
        • Getting Started with Kinetis SDK (KSDK) v.2.0
        • Kinds of user guides and readme.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)