KSDK version 1.3.0 or 2.0.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK version 1.3.0 or 2.0.0?

Jump to solution
6,097 Views
bernadettmarton
Contributor I

Hi All,

Can somebody tell me, which version of KSDK supports the KE02 Familly? I am starting to work with FRDM-KE02Z Board. Thanks in advance!

Labels (1)
0 Kudos
Reply
1 Solution
5,847 Views
zhaowum
Contributor II

maybe you can start your work with the help of PE, Try follow this link https://community.nxp.com/thread/385482 

 I found it can help me to create the right project and go on my coding.

View solution in original post

0 Kudos
Reply
6 Replies
5,848 Views
zhaowum
Contributor II

maybe you can start your work with the help of PE, Try follow this link https://community.nxp.com/thread/385482 

 I found it can help me to create the right project and go on my coding.

0 Kudos
Reply
5,846 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Bernadett Marton​,

unfortunately there is no support of KE and KEA family in KSDK.

But you can take a look  at QSP and sample codes located here Kinetis E Series Freedom Development Platform|NXP

I hope this helps.

In case of any issue, please let me know.

Best Regards,

Iva

0 Kudos
Reply
5,798 Views
skaval99
Contributor I

Dear friends

Facing a peculiar problem in MKE02Z64VLH4 based custom board being debugged through FRDM-02Z board running J-Link open SDA app.

The software in custom board works excellently as long as connected to debugger but stops working as soon as debugger is disconnected. Also system does not boot up if not connected to debugger.

IDE used is MCUXpresso ( v11.0.1 [Build 2563] [2019-09-01]) with project generated from copying an SDK_2.x_FRDM-02Z40M, ver 2.6.0 based project named "frdmke02z40m_ftm_timer"

Search on the forum so far has not provided any workable solution. 

Any help or ideas from NXP team would be highly appreciated.

Regards

0 Kudos
Reply
5,796 Views
ErichStyger
Specialist I

Hi @skaval99 ,

that "does not work if no debugger attached" sounds like you are using semihosting functionality? Check if you are using printf() in any variant.

If you do not have a dedicated hardfault handler for this your application will raise a hardfault.

You might use the following hardfault handler in

https://github.com/ErichStyger/McuOnEclipseLibrary/blob/master/lib/src/McuHardFault.c

which does a detection if the hardfault is coming from semihosting or not.

The SDK 2.x does come with a similar handler too.

 

I hope this helps,

Erich

0 Kudos
Reply
5,785 Views
skaval99
Contributor I

Dear Erich,

Many thanks for your response and suggestion.

The problem has been resolved as it was being caused by floating inputs of 3.3V to 5V logic level shifters (in RST & CLK lines) implemented in my custom board (working at 5V) to carry out programming/debugging with FRDM-KE02Z board working at 3,3V .

Rest of the system and software is working really well. MCUXpresso and FRDM-KE02Z as debugger for development with MKE02Z64VLH4 chip are working without any issues.

Rgrds 

Kaval

0 Kudos
Reply
5,783 Views
ErichStyger
Specialist I

Hi @skaval99 ,

great to hear that this has been resolved!

I guess I should add that one to my growing list on https://mcuoneclipse.com/2016/07/01/board-bring-up-tips-gdb-logs-and-traces-in-eclipse/

 

Erich

0 Kudos
Reply