KSDK Project Generator do not install - is not a win 32  application.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KSDK Project Generator do not install - is not a win 32  application.

2,218 次查看
viktordementiev
Contributor I

So.  I try to install   Kinetis SDK Project Generator Tool. I get it from this site (step 4):  FRDM-K22F|Freedom Development Board|Kinetis|NXP

. But if I try to run ../Windows/KSDK_Project_Generator.exe from downloaded archive I got message:

KSDK Project Generator  - is not a win 32  application. I try to do it under XP and Win 7 witn the same resuilts. Whats wrong?

标签 (1)
0 项奖励
回复
3 回复数

1,789 次查看
viktordementiev
Contributor I

Not_a_app_win32.bmp

It is under Win XP

Yes - it's V2.0 .

So ,  it is under Win 7:

Not_a_win32_win7.bmp

May be V2.0 is for 64 bit OS only?

0 项奖励
回复

1,789 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Viktor.

Thank you for your valuable feedback but I have 2 comments.

1) please work with the newest Project Generator Tool Kinetis SDK Project Generator Tool

2) Target systems configurations are following:

This product has been tested on the following system configurations:

8.1 Operating Systems

• Windows 7 32-bit,

• Linux Ubuntu 14.10 64-bit

• Mac OS X 10.10 or 10.11

so it should work on your Win7 32-bit.

Please can you rewrite the error message for me?

Thank you.

Have a nice day!

Iva

0 项奖励
回复

1,789 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Viktor,

thank you for your feedback.

Please, do you use the newest version KSDK Project Generator Tool?

New Kinetis SDK Project Generator v2 is available!

Please, can you upload a print screen of the issue?

Thank you.

Have a nice day.

Iva

0 项奖励
回复