KSDK 2.0 usb_host_config.h for KL26Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KSDK 2.0 usb_host_config.h for KL26Z

跳至解决方案
1,788 次查看
enchanter
Contributor I

I would like to use the USB host on a KL27Z to write a USB flash drive. I downloaded the KSDK 2.0 for the FRDM-KL27Z board and IAR running on Windows. In the second step in the USB Stack User's Guide (section 4.2.2.1), the file usb_host_config.h is copied to an application directory; however, there is no usb_host_config.h file in the KDSK. All of the KDSK examples are for the USB device. Where is usb_host_config.h for the KL27Z?

标签 (1)
标记 (1)
1 解答
1,560 次查看
DavidS
NXP Employee
NXP Employee

Hi Tim,

The KL27 is USB device only (crystal-less USB).

The KL26 and KL46 (USB OTG Host and Device support) will have KSDK_v2 support end of March per Introducing Kinetis SDK v2 .

Regards,

David

在原帖中查看解决方案

1 回复
1,561 次查看
DavidS
NXP Employee
NXP Employee

Hi Tim,

The KL27 is USB device only (crystal-less USB).

The KL26 and KL46 (USB OTG Host and Device support) will have KSDK_v2 support end of March per Introducing Kinetis SDK v2 .

Regards,

David