KSDK 2.0 for Kinetis V series.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK 2.0 for Kinetis V series.

1,257件の閲覧回数
arimendes
Contributor III

Hi,

KSDK 2.0 for Kinetis V series: Already has a date for the release?

I know that it is Mid July, I only want to avoid to enter every day in the KSKD build page to see if it is already there.

 

Ari.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,034件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Ari.

Thank you for your interest.

The release date was shifted. It is expected during the August.

Thank you for your patience.

Have a great day.

Iva

0 件の賞賛
返信

1,034件の閲覧回数
arimendes
Contributor III

Iva,

All I need to start my development is a MKV58F1M0VLL12 KSDK 2.0 project template for EWARM. Setting for 240MHZ CPU clock and 120MHZ peripheral clock with all caches enabled. Can you send to me a beta version of it?

Thanks.

Ari.

De: ivadorazinova

Enviada em: quarta-feira, 13 de julho de 2016 10:00

Para: Ari Mendes

Assunto: Re: - KSDK 2.0 for Kinetis V series.

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

KSDK 2.0 for Kinetis V series.

reply from Iva <https://community.nxp.com/people/ivadorazinova?et=watches.email.thread> Dorazinova in Kinetis Software Development Kit - View <https://community.nxp.com/message/811479?et=watches.email.thread#comment-811479> the full discussion

0 件の賞賛
返信

1,034件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Ari,

You will receive this Beta version soon.

Have a great day!

Iva

0 件の賞賛
返信