KSDK 2.0 for Kinetis V series.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK 2.0 for Kinetis V series.

1,661 Views
arimendes
Contributor III

Hi,

KSDK 2.0 for Kinetis V series: Already has a date for the release?

I know that it is Mid July, I only want to avoid to enter every day in the KSKD build page to see if it is already there.

 

Ari.

Labels (1)
0 Kudos
Reply
3 Replies

1,438 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Ari.

Thank you for your interest.

The release date was shifted. It is expected during the August.

Thank you for your patience.

Have a great day.

Iva

0 Kudos
Reply

1,438 Views
arimendes
Contributor III

Iva,

All I need to start my development is a MKV58F1M0VLL12 KSDK 2.0 project template for EWARM. Setting for 240MHZ CPU clock and 120MHZ peripheral clock with all caches enabled. Can you send to me a beta version of it?

Thanks.

Ari.

De: ivadorazinova

Enviada em: quarta-feira, 13 de julho de 2016 10:00

Para: Ari Mendes

Assunto: Re: - KSDK 2.0 for Kinetis V series.

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

KSDK 2.0 for Kinetis V series.

reply from Iva <https://community.nxp.com/people/ivadorazinova?et=watches.email.thread> Dorazinova in Kinetis Software Development Kit - View <https://community.nxp.com/message/811479?et=watches.email.thread#comment-811479> the full discussion

0 Kudos
Reply

1,438 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Ari,

You will receive this Beta version soon.

Have a great day!

Iva

0 Kudos
Reply