KSDK 1.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK 1.3

Jump to solution
3,176 Views
billnd
Contributor IV

There seems to be quite a jump between KSDK 1.1 and KSDK 1.2, and many people finding it hard work to update existing 1.1 projects to 1.2. So is 1.2 to 1.3 likely to be such a big jump, or has the KSDK started to settle down?

 

We're looking at porting existing non-KSDK projects over to the KSDK, and don't want to have to port to 1.2, and then port from 1.2 to 1.3. I read somewhere that KSDK 1.3 is due out in a couple of months.

 

Is there a public list of changes that are to be incorporated into 1.3?

 

Cheers,

NDBill

Labels (1)
Tags (1)
1 Solution
2,273 Views
anthony_huereca
NXP Employee
NXP Employee

Hi,

  For anyone interested in this, there were no major changes in the API for KSDK 1.3 compared to KSDK 1.2. The biggest changes are just the addition of newly supported boards/devices, and some new peripherals that are now supported too.

The KSDK 1.3 release notes have the full details, including "Chapter 8 Change Log" which lists the minimal API changes (mostly to add new APIs).

-Anthony

View solution in original post

3 Replies
2,274 Views
anthony_huereca
NXP Employee
NXP Employee

Hi,

  For anyone interested in this, there were no major changes in the API for KSDK 1.3 compared to KSDK 1.2. The biggest changes are just the addition of newly supported boards/devices, and some new peripherals that are now supported too.

The KSDK 1.3 release notes have the full details, including "Chapter 8 Change Log" which lists the minimal API changes (mostly to add new APIs).

-Anthony

2,273 Views
ivadorazinova
NXP Employee
NXP Employee

Hello billnd,

I checked the information for you, and unfortunately there is no chance now to get Release Note for KSDK 1.3.

Now it is not final version and we have still worked on it.

Have a great day!

Iva

0 Kudos
Reply
2,273 Views
ivadorazinova
NXP Employee
NXP Employee

Hello billnd,

thank you for your interest, we expect KSDK 1.3 in Q3 (by end of Sept), 

I will pass it to SW team and tell you more,

Regards!

Iva

0 Kudos
Reply