KSDK 1.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,196件の閲覧回数
billnd
Contributor IV

There seems to be quite a jump between KSDK 1.1 and KSDK 1.2, and many people finding it hard work to update existing 1.1 projects to 1.2. So is 1.2 to 1.3 likely to be such a big jump, or has the KSDK started to settle down?

 

We're looking at porting existing non-KSDK projects over to the KSDK, and don't want to have to port to 1.2, and then port from 1.2 to 1.3. I read somewhere that KSDK 1.3 is due out in a couple of months.

 

Is there a public list of changes that are to be incorporated into 1.3?

 

Cheers,

NDBill

ラベル(1)
タグ(1)
1 解決策
2,293件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi,

  For anyone interested in this, there were no major changes in the API for KSDK 1.3 compared to KSDK 1.2. The biggest changes are just the addition of newly supported boards/devices, and some new peripherals that are now supported too.

The KSDK 1.3 release notes have the full details, including "Chapter 8 Change Log" which lists the minimal API changes (mostly to add new APIs).

-Anthony

元の投稿で解決策を見る

3 返答(返信)
2,294件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi,

  For anyone interested in this, there were no major changes in the API for KSDK 1.3 compared to KSDK 1.2. The biggest changes are just the addition of newly supported boards/devices, and some new peripherals that are now supported too.

The KSDK 1.3 release notes have the full details, including "Chapter 8 Change Log" which lists the minimal API changes (mostly to add new APIs).

-Anthony

2,293件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello billnd,

I checked the information for you, and unfortunately there is no chance now to get Release Note for KSDK 1.3.

Now it is not final version and we have still worked on it.

Have a great day!

Iva

0 件の賞賛
返信
2,293件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello billnd,

thank you for your interest, we expect KSDK 1.3 in Q3 (by end of Sept), 

I will pass it to SW team and tell you more,

Regards!

Iva

0 件の賞賛
返信