KSDK 1.3 for K22FN128-100Mhz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK 1.3 for K22FN128-100Mhz

1,054 Views
HeMyFAE
NXP Employee
NXP Employee


Dear KSDK 1.3 support team,

 

My customer changed the MCU on the FRDM-K22 from a K22FN512-120 to a K22FN128-100Mhz.

Using the KSDK generator from the web, I generated specific KSDK1.3 for K22FN128 to support the new MCU but the demo code such as Hello World, Bubble, nor USB HID are not working.

Below is the error messages in the Console window.

 

 

To verified that new K22FN128 MCU is ok, I loaded a K22FN128-100Mhz  LED demo code from the Kboot 2.0 package to verify the FN22FN128 and it seems to be working fine.

 

148479_148479.pngdebug_screen.png

Labels (1)
0 Kudos
Reply
1 Reply

913 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mai,

Do you meaning change the chip K22FN512VLH12 to K22FN128-100Mhz in to FRDM-K22 board?

Then use the ksdk demo about K22FN128-100Mhz chip ?

If yes, i recommend you first test one simple without ksdk project on it , check whether it can work well .

Hope it helps

Alice

0 Kudos
Reply