KSDK 1.1.0 Installation Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KSDK 1.1.0 Installation Problem

跳至解决方案
4,113 次查看
lmg
Contributor III

I'm attempting to move to KSDK 1.1.0 (from 1.0.0).

 

I uninstalled old version of both KSDK and KDS 2.0.0.

 

Reinstalled KDS 2.0.0

 

Installed KSDK 1.1.0

 

Imported KSDK Software into KDS (per "Getting Started" .pdf)

 

Imported the appropriate library (per "Getting Started" )

 

Attempted to build the debug configuration of the library and got 95 errors.

 

20043_20043.jpgLibrary Error Message.JPG.jpg

 

What am I missing?

 

Thanks.

 

~LMG

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,856 次查看
lmg
Contributor III

Thanks for the reply David.  KSDK_PATH is correct. I believe this was automatic since I started with a clean installation.

But I did find this:

No Rule to Make Target in KDS

It points out that when importing a library, you have to un-check "Copy projects into workspace". If you copy the files into the workspace, the links to other modules don't work.

Having done that, I'm in good shape.

Thanks.

~LMG

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,856 次查看
DavidS
NXP Employee
NXP Employee

Did you update your KDS environmental variable?

Regards,

David

3,857 次查看
lmg
Contributor III

Thanks for the reply David.  KSDK_PATH is correct. I believe this was automatic since I started with a clean installation.

But I did find this:

No Rule to Make Target in KDS

It points out that when importing a library, you have to un-check "Copy projects into workspace". If you copy the files into the workspace, the links to other modules don't work.

Having done that, I'm in good shape.

Thanks.

~LMG

0 项奖励
回复