KSDK 1.1.0 Installation Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK 1.1.0 Installation Problem

Jump to solution
4,014 Views
lmg
Contributor III

I'm attempting to move to KSDK 1.1.0 (from 1.0.0).

 

I uninstalled old version of both KSDK and KDS 2.0.0.

 

Reinstalled KDS 2.0.0

 

Installed KSDK 1.1.0

 

Imported KSDK Software into KDS (per "Getting Started" .pdf)

 

Imported the appropriate library (per "Getting Started" )

 

Attempted to build the debug configuration of the library and got 95 errors.

 

20043_20043.jpgLibrary Error Message.JPG.jpg

 

What am I missing?

 

Thanks.

 

~LMG

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,757 Views
lmg
Contributor III

Thanks for the reply David.  KSDK_PATH is correct. I believe this was automatic since I started with a clean installation.

But I did find this:

No Rule to Make Target in KDS

It points out that when importing a library, you have to un-check "Copy projects into workspace". If you copy the files into the workspace, the links to other modules don't work.

Having done that, I'm in good shape.

Thanks.

~LMG

View solution in original post

0 Kudos
Reply
2 Replies
3,757 Views
DavidS
NXP Employee
NXP Employee

Did you update your KDS environmental variable?

Regards,

David

3,758 Views
lmg
Contributor III

Thanks for the reply David.  KSDK_PATH is correct. I believe this was automatic since I started with a clean installation.

But I did find this:

No Rule to Make Target in KDS

It points out that when importing a library, you have to un-check "Copy projects into workspace". If you copy the files into the workspace, the links to other modules don't work.

Having done that, I'm in good shape.

Thanks.

~LMG

0 Kudos
Reply