KSDK 1.1.0 Installation Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK 1.1.0 Installation Problem

ソリューションへジャンプ
3,971件の閲覧回数
lmg
Contributor III

I'm attempting to move to KSDK 1.1.0 (from 1.0.0).

 

I uninstalled old version of both KSDK and KDS 2.0.0.

 

Reinstalled KDS 2.0.0

 

Installed KSDK 1.1.0

 

Imported KSDK Software into KDS (per "Getting Started" .pdf)

 

Imported the appropriate library (per "Getting Started" )

 

Attempted to build the debug configuration of the library and got 95 errors.

 

20043_20043.jpgLibrary Error Message.JPG.jpg

 

What am I missing?

 

Thanks.

 

~LMG

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,714件の閲覧回数
lmg
Contributor III

Thanks for the reply David.  KSDK_PATH is correct. I believe this was automatic since I started with a clean installation.

But I did find this:

No Rule to Make Target in KDS

It points out that when importing a library, you have to un-check "Copy projects into workspace". If you copy the files into the workspace, the links to other modules don't work.

Having done that, I'm in good shape.

Thanks.

~LMG

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,714件の閲覧回数
DavidS
NXP Employee
NXP Employee

Did you update your KDS environmental variable?

Regards,

David

3,715件の閲覧回数
lmg
Contributor III

Thanks for the reply David.  KSDK_PATH is correct. I believe this was automatic since I started with a clean installation.

But I did find this:

No Rule to Make Target in KDS

It points out that when importing a library, you have to un-check "Copy projects into workspace". If you copy the files into the workspace, the links to other modules don't work.

Having done that, I'm in good shape.

Thanks.

~LMG

0 件の賞賛
返信