KL03 flsl_flash error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL03 flsl_flash error

Jump to solution
1,880 Views
Lupo
Contributor III

Hello,

developing with a KL03 processor using the KDS v3.00 with KDSK 1.20 and using the flsl_flash component I am facing  a strange error.

 

Stepping manually (F5/F6) through the instructions of the function FlashCommandSequence() in file FlashCommandSequence.c, the flash memory gets correctly written or erased but if program is running normally, processor does never go over the following loop and resets:

while(0x0U == (REG_BIT_GET(temp, FTFx_SSD_FSTAT_CCIF)))     /* wait till CCIF bit is set */

 

Processor uses the internal clock and watchdog is disabled; before starting the flash instruction CCIF is high and ACCERR and FPVIOL flags are low; adding delays does not help.

 

What else? Thanks for any suggestion, Michael

Labels (1)
0 Kudos
Reply
1 Solution
1,737 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Michael Hauptman,

      Did you relocate your FlashCommandSequence function to  the RAM by using  g_FlashLaunchCommand = (pFLASHCOMMANDSEQUENCE)RelocateFunction((uint32_t)ramFunc , 0x100 ,(uint32_t)FlashCommandSequence);?

    Besides, please attach your problem project, I need to check it.

Waiting for your reply


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,738 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Michael Hauptman,

      Did you relocate your FlashCommandSequence function to  the RAM by using  g_FlashLaunchCommand = (pFLASHCOMMANDSEQUENCE)RelocateFunction((uint32_t)ramFunc , 0x100 ,(uint32_t)FlashCommandSequence);?

    Besides, please attach your problem project, I need to check it.

Waiting for your reply


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,737 Views
Lupo
Contributor III

Hi Jingjing,

you are right! I am not fully confident with the KDSK and I missed that instruction...

Btw the classic PEx in KDS or CW is very, very, better than the KDSK version to help developpers!

Many thanks, Michael

0 Kudos
Reply