KDS MK66 USB ISSUE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS MK66 USB ISSUE

1,396件の閲覧回数
kapilkushe
Contributor I

Sir,

     I want to write code for dual fat i.e. msd & sd-card. I am using mk66 controller. I have refer mk65 kds example code. I successfully port it for mk66. but its not working. if I manually debug the code then its device state of usb is not changing. so I am stuck there . how can I proceed further.. thanks in advance

ラベル(1)
0 件の賞賛
返信
1 返信

1,154件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Kapil,

Debuggin USB application without using an USB sniffer is quite hard because USB clocks are stopped and USB transactions cannot be completed correctly. I would strongly recommend you to use an USB sniffer.

Does USB device cannot be recognized in PC? or what error can you see? Common errors are listed here:

KDS/KSDK K20 USB Driver Mutex Problem

usb_dev_msd_cdc example problems

PE-generated USB code does not seem to work

Hope this helps!

Regards,

Isaac Avila

0 件の賞賛
返信