Is there any tool like PE in SDK 2.0?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any tool like PE in SDK 2.0?

1,303 次查看
zhongshen
Contributor III

I have used PE with SDK 1.3 with KDS 3.0, so that it is easy to add the component to the project and configure the pins and initiate the component, let me to focus the program of application. And now there is KDS 3.2 and SDK 2.0, but there is not PE support. I need to study the datasheet and understand the registers on the component to initiate the pinmux and set the registers.

 

Is there any tool like PE in SDK 2.0  to make program easy?

 

Thanks.

 

Zhong Shen

标签 (1)
0 项奖励
回复
4 回复数

1,051 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Zhong Shen,

we prepared configuration tools, which will be available soon.

I will keep you informed,

Best Regards,

Iva

0 项奖励
回复

1,051 次查看
zhongshen
Contributor III

Hi Iva,

Any update?

0 项奖励
回复

1,051 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello,

no, these tools are no available just now. But it will be ready soon.

You will see it under Tools in kex.freescale.com

tools.png

At the moment is available Power Estimation Tool.

I will keep you informed.

Have a nice day.

Iva

0 项奖励
回复

1,051 次查看
zhongshen
Contributor III

Thanks.

0 项奖励
回复