Is there any tool like PE in SDK 2.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any tool like PE in SDK 2.0?

1,327件の閲覧回数
zhongshen
Contributor III

I have used PE with SDK 1.3 with KDS 3.0, so that it is easy to add the component to the project and configure the pins and initiate the component, let me to focus the program of application. And now there is KDS 3.2 and SDK 2.0, but there is not PE support. I need to study the datasheet and understand the registers on the component to initiate the pinmux and set the registers.

 

Is there any tool like PE in SDK 2.0  to make program easy?

 

Thanks.

 

Zhong Shen

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,075件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Zhong Shen,

we prepared configuration tools, which will be available soon.

I will keep you informed,

Best Regards,

Iva

0 件の賞賛
返信

1,075件の閲覧回数
zhongshen
Contributor III

Hi Iva,

Any update?

0 件の賞賛
返信

1,075件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello,

no, these tools are no available just now. But it will be ready soon.

You will see it under Tools in kex.freescale.com

tools.png

At the moment is available Power Estimation Tool.

I will keep you informed.

Have a nice day.

Iva

0 件の賞賛
返信

1,075件の閲覧回数
zhongshen
Contributor III

Thanks.

0 件の賞賛
返信