IntFLASH component

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IntFLASH component

2,580 Views
dongshengwang
Contributor I

Hi

 

I am porting a project to FRDM-K64F. I want to read / write the internal flash memory at runtime. In this community I found a solution, mentioned to use IntFLASH component. But I can not find it. My development environment is KDS_1.1.1 and MQX_KSDK_1.0.0.

 

Than you!

Labels (1)
0 Kudos
Reply
3 Replies

2,355 Views
BlackNight
NXP Employee
NXP Employee

It look you are using the Kinetis SDK? Then all the *_LDD and other non SDK components are not available any more, if you have an SDK project.

Erich

0 Kudos
Reply

2,355 Views
dongshengwang
Contributor I

Hi Erich

Thanks for your answer. The Kinetis SDK offer the API function to write / read the internal flash? If so, How can I use it and config the internal flash memory.

Regards,

Dongsheng Wang

0 Kudos
Reply

2,355 Views
terry_lv
NXP Employee
NXP Employee

Hi,

     You can refer to flash_demo under demo directory for reference.

     Thanks!

Best regards

Terry

0 Kudos
Reply