IntFLASH component

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IntFLASH component

2,557件の閲覧回数
dongshengwang
Contributor I

Hi

 

I am porting a project to FRDM-K64F. I want to read / write the internal flash memory at runtime. In this community I found a solution, mentioned to use IntFLASH component. But I can not find it. My development environment is KDS_1.1.1 and MQX_KSDK_1.0.0.

 

Than you!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,332件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It look you are using the Kinetis SDK? Then all the *_LDD and other non SDK components are not available any more, if you have an SDK project.

Erich

0 件の賞賛
返信

2,332件の閲覧回数
dongshengwang
Contributor I

Hi Erich

Thanks for your answer. The Kinetis SDK offer the API function to write / read the internal flash? If so, How can I use it and config the internal flash memory.

Regards,

Dongsheng Wang

0 件の賞賛
返信

2,332件の閲覧回数
terry_lv
NXP Employee
NXP Employee

Hi,

     You can refer to flash_demo under demo directory for reference.

     Thanks!

Best regards

Terry

0 件の賞賛
返信