Input capture and dual edge capture in KSDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Input capture and dual edge capture in KSDK?

1,222 Views
therealfreegeek
Contributor IV

Can anyone say when it will be supported?

Labels (1)
0 Kudos
Reply
2 Replies

897 Views
therealfreegeek
Contributor IV

Looks like I can answer this one myself now.

It seems like NXP have released KSDK 2.0 without any announcement or fanfare on 28th Jan, the day I posted the above message.

I found this in the api document.

23.2.3 Input capture operations

The function FTM_SetupInputCapture()sets up an FTM channel for input capture. The
user can specify the capture edge and a filter value to be used when processing
the input signal.

The function FTM_SetupDualEdgeCapture()can be used to measure the pulse width of a
signal. A channel pair is used during capture with the input signal coming
through a channel n. The user can specify whether to use one-shot or continuous
capture, the capture edge for each channel, and any filter value to be used when
processing the input signal.

0 Kudos
Reply

897 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Sorry for the delayed response. You are right that both modes should be supported in KSDK v2.0.

If you find any problems using these modes please let us know.

Regards!

Jorge Gonzalez

0 Kudos
Reply