I have no processors or boards available when creating a new project in KDS V2.0. I tried reinstalling KDS, still the same. I am running Win 10 64 bit on a core i7. I want to use my FRDM KL25Z board to begin with

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have no processors or boards available when creating a new project in KDS V2.0. I tried reinstalling KDS, still the same. I am running Win 10 64 bit on a core i7. I want to use my FRDM KL25Z board to begin with

1,614件の閲覧回数
petersommer
Contributor I

The window says "contains processors" or "contains board support" but there is nothing there. I can'@t move on from here.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,433件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Peter!

1) Please, go to https://nxp.flexnetoperations.com/control/frse/product?entitlementId=123521727&lineNum=1&authContact...  and download the newest KDS v.3.2.0, please see also New Kinetis Design Studio v3.2.0 available

2) do you want to create new KSDK project? If yes, you should have downloaded package for your KL25Z from http://kex.freescale.com/ with the procedure described here How to: install KSDK 2.0 and create new project via wizard or project generator tool, please see New Kinetis SDK Project Generator v2 is available!

wizard.png

Please let me know in case of any issue,

Best Regards,

Iva

0 件の賞賛
返信

1,433件の閲覧回数
petersommer
Contributor I

It is actually KDS V3.2. sorry.

0 件の賞賛
返信