How to store flexNVM data on KDS/KSDK/PEx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to store flexNVM data on KDS/KSDK/PEx

1,600 Views
yarannan
Contributor III

Hi,

I am pretty new to this concept. Hopefully someone can help me,.

1. The chip i am using MK20DX256VLL10

2. The tool i am using is KDS3.0 with KSDK1.2 and PEx

3. I try to take a look at demo code but it is about program flash, not abou dataFlash/FlexNVM or EEEPROM.

I also looked at K20RM and AM4282. I think i understand the concept but the code that i made is still not working.

4. I tried to write this single feature on KDS2.0 + PEx to make sure i understand the concept. It works well.

Below are steps that I did:

100483_100483.JPG1.JPG

Change the flash configuration of CPU

Add fsl_flash component from PEx

 

100496_100496.JPG2.JPG

 

The C90TFS base address is 0x40020000 Program flash address: 0x00000000.

I found out at generated flash file, EEPROM and Dflash size is 0. I coudnt modify it.

I used the code below to try to write four bytes data into Dflash whose address is 0x10000000

It doesnt throw me error but i just couldnt read it back.

Could anyone spot anything wrong?

 

Thanks,

Yaran

Original Attachment has been moved to: main.c.zip

Original Attachment has been moved to: flash_mk20.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,402 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Nan,

1. By default , the linker file do not include the FlexNVM memory define, so we need configure it by hand.

I see you have add it in the PE , please enable it :

pastedImage_0.png

2.  Before program flash memory , please first erase it .

3. Please configure the 23 bit of  flexNVM address you wan to operate to 1, you can see the information on the Reference manual :

page 649 ->

pastedImage_1.png

Hope it helps

Alice

0 Kudos
Reply