Dear All:
I have a custom board made already with MK60FN1M0VLQ15 and the firmware has been developed by CW10.6 with MQX4.1. In the near future, we are going to use KDS 3.0.0 and KSDK 1.2.0 for new board in new project. Currently, I am using this existing custom board as my starting learning point. There are so many resources and nor sure which way to go:
1. If I understand correct, I need to select a closed evaluation board as a base, and create project by "KSDK project generator". I am not sure which evaluation board I should start from?
2. Or if there is a better way to start a custom board?
3. How do I change CPU clock setting from original supported to 150MHz?
If anyone had experience, please let me know any suggestion. Thank you very much.