Hi
I am bringing up the custom board designed based on K64 micro. During the bring up I used Tower K64 based projects for USB and ethernet interfaces. And KDS 3.0 and KDSK 1.2 with processor expert for bringing up peripherals interfaces like UART, SPI etc.
Now I need to create a project exclusively for my custom board with USB, ethernet, SD CARD, file system support on MQX platform.
Please share me any document which explains the procedure. Most of the time I can see the documents which written for KDSK 1.2, is referring to KDSK 1.1 folder structure.
Basically I do not want to modify the TowerK64 folders for my custom board.
Would greatly appreciate any help on this.
Regards
Riju