Hi all, is there an way to programm a seperate KEA128 controller on a custom designed board via the OpenSDA interface of another KEA128 evaluation board? Any help will be appreciated.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi all, is there an way to programm a seperate KEA128 controller on a custom designed board via the OpenSDA interface of another KEA128 evaluation board? Any help will be appreciated.

773件の閲覧回数
maharajshreekum
Contributor III

I have a kea 128 controller embedded on a custom designed PCB for my application. I also have TRK KEA 128 evaluation board. My requirement is that I want to program my PCB KEA controleer with Open SDA interace of the evalaution board, using the pins of the SWD KEA programming connector (J12) on the evaluation board. 

 

Also, I am using Keil V5.16 to program the KEA evalution board using the onboard Open SDA debugger supported by PE debugger.

 

Is there a way to it.

 

Pls help

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)