Has anyone managed to use KSDK CDC Example with Windows WriteFile?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone managed to use KSDK CDC Example with Windows WriteFile?

3,315 Views
ashesman
Contributor III

Hi,

 

I have tried to use WriteFile to send a short string of eight characters from a Delphi program and c#.  Both of them lockup and writefile never returns .  However, using a terminal program (realterm), it works perfectly!

 

A breakpoint on the CDC callback is never hit when writefile is called.  However, it is hit many times when the port is opened!

 

Has anyone managed to use the KSDK CDC with a windows program that uses WriteFile?  Specifically I am using the Composite CDC and MSC example on K24.  

 

HEEELLLLPPPP!!!!!!!!!

 

Ashley

Labels (1)
0 Kudos
Reply
4 Replies

3,046 Views
PitOn
Contributor III

#region CDC Support
public class UsbDeviceMonitor
{
private ManagementEventWatcher plugInWatcher;
private ManagementEventWatcher unPlugWatcher;
private const string MyDeviceDescription = @"My Device Description";

~UsbDeviceMonitor()
{
Dispose();
}

public void Dispose()
{
if (plugInWatcher != null)
try
{
plugInWatcher.Dispose();
plugInWatcher = null;
}
catch (Exception) { }

if (unPlugWatcher == null) return;
try {
unPlugWatcher.Dispose();
unPlugWatcher = null;
}
catch (Exception) { }
}

public void Start()
{
const string plugInSql = "SELECT * FROM __InstanceCreationEvent WITHIN 1 WHERE TargetInstance ISA 'Win32_PnPEntity'";
const string unpluggedSql = "SELECT * FROM __InstanceDeletionEvent WITHIN 1 WHERE TargetInstance ISA 'Win32_PnPEntity'";

var scope = new ManagementScope("root\\CIMV2") { Options = { EnablePrivileges = true } };

var pluggedInQuery = new WqlEventQuery(plugInSql);
plugInWatcher = new ManagementEventWatcher(scope, pluggedInQuery);
plugInWatcher.EventArrived += HandlePluggedInEvent;
plugInWatcher.Start();

var unPluggedQuery = new WqlEventQuery(unpluggedSql);
unPlugWatcher = new ManagementEventWatcher(scope, unPluggedQuery);
unPlugWatcher.EventArrived += HandleUnPluggedEvent;
unPlugWatcher.Start();
}

private void HandleUnPluggedEvent(object sender, EventArrivedEventArgs e)
{
var description = GetDeviceDescription(e.NewEvent);
foreach (COMPortInfo comPort in COMPortInfo.GetCOMPortsInfo())
{
// comboBoxPort.Items.Add(string.Format("{0} – {1}", comPort.Name, comPort.Description));
// this.comboBoxPort.Items.Add(string.Format("{0}", comPort.Description));
}
if (description.Equals(MyDeviceDescription)) {
// Take actions here when the device is unplugged
}
}

private void HandlePluggedInEvent(object sender, EventArrivedEventArgs e)
{
var description = GetDeviceDescription(e.NewEvent);
if (description.Equals(MyDeviceDescription)){
// Take actions here when the device is plugged in
}
}

private static string GetDeviceDescription(ManagementBaseObject newEvent)
{
var targetInstanceData = newEvent.Properties["TargetInstance"];
var targetInstanceObject = (ManagementBaseObject)targetInstanceData.Value;
if (targetInstanceObject == null) return "";

var description = targetInstanceObject.Properties["Description"].Value.ToString();
return description;
}
}

internal class ProcessConnection
{
public static ConnectionOptions ProcessConnectionOptions()
{
ConnectionOptions options = new ConnectionOptions();
options.Impersonation = ImpersonationLevel.Impersonate;
options.Authentication = AuthenticationLevel.Default;
options.EnablePrivileges = true;
return options;
}

public static ManagementScope ConnectionScope(string machineName, ConnectionOptions options, string path)
{
ManagementScope connectScope = new ManagementScope();
connectScope.Path = new ManagementPath(@"\\" + machineName + path);
connectScope.Options = options;
connectScope.Connect();
return connectScope;
}
}
//===================================================
public class COMPortInfo
{
public string Name { get; set; }
public string Description { get; set; }

public COMPortInfo() { }

public static List<COMPortInfo> GetCOMPortsInfo()
{
List<COMPortInfo> comPortInfoList = new List<COMPortInfo>();

ConnectionOptions options = ProcessConnection.ProcessConnectionOptions();
ManagementScope connectionScope = ProcessConnection.ConnectionScope(Environment.MachineName, options, @"\root\CIMV2");

ObjectQuery objectQuery = new ObjectQuery("SELECT * FROM Win32_PnPEntity WHERE ConfigManagerErrorCode = 0");
ManagementObjectSearcher comPortSearcher = new ManagementObjectSearcher(connectionScope, objectQuery);

using (comPortSearcher)
{
string caption = null;
foreach (ManagementObject obj in comPortSearcher.Get())
{
if (obj != null)
{
object captionObj = obj["Caption"];
if (captionObj != null)
{
caption = captionObj.ToString();
if (caption.Contains("(COM"))
{
COMPortInfo comPortInfo = new COMPortInfo();
comPortInfo.Name = caption.Substring(caption.LastIndexOf("(COM")).Replace("(", string.Empty).Replace(")",
string.Empty);
comPortInfo.Description = caption;
comPortInfoList.Add(comPortInfo);
}
}
}
}
}
return comPortInfoList;
}
}

/*********************************************************************
* Base Class
**********************************************************************/
public class MySerialPort : SerialPort
{
private const int DataSize = 256; //
private readonly byte[] _bufer = new byte[DataSize];
private int _stepIndex = 0;
/// </summary>
public MySerialPort()
: base()
{

// Set parameter
base.BaudRate = 115200;
base.DataBits = 8;
base.StopBits = StopBits.One;
base.Parity = Parity.None;
base.ReadTimeout = 1000;
base.DtrEnable = true;

_stepIndex = 0;
if (base.IsOpen)
base.Close();

// Event Data Received;
base.DataReceived += SerialPort_DataReceived;
// Event Error
base.ErrorReceived += SerialPort_ErrorReceived;
}
//===================================================================================
void SerialPort_ErrorReceived(object sender, SerialErrorReceivedEventArgs e)
{
// if(e.EventType == SerialError.TXFull).....
MessageBox.Show("Error recieved: " + e.EventType);
}
// Open Port "com1"
public void Open(string portName)
{
try
{
if (base.IsOpen)
{
base.Close();
}
base.PortName = portName;
base.Open();
base.DiscardInBuffer();
_stepIndex = 0;
}
catch { }

_stepIndex = 0;
}
//------> Out Data <-------
public void Send_CmdData(byte[] buffer)
{

byte CS = 0;
try
{
for (byte i = 0; i < buffer[1] - 1; i++)
CS += buffer[i];

buffer[buffer[1] - 1] = (byte)(~CS + 1);
base.Write(buffer, 0, buffer[1]);
}
catch { }
}

// --Test Input Data
void SerialPort_DataReceived(object sender, SerialDataReceivedEventArgs e)
{
var port = (SerialPort)sender;
try
{
// 
int buferSize = port.BytesToRead;
for (int i = 0; i < buferSize; ++i)
{
// 
_bufer[_stepIndex++] = (byte)port.ReadByte();
if (_stepIndex == 1)

if (0x05 != _bufer[0]) _stepIndex = 0;
else continue;
}
else 
if ((_stepIndex >= DataSize) || (_stepIndex == _bufer[1]))
{
byte CS = 0;
for (int j = 0; _stepIndex != 0; _stepIndex--)
CS += _bufer[j++];
if (CS == 0)
{
_stepIndex = 0; // .. 
Egor_Host.Egor.CallBackMy.callbackEventHandler(_bufer);
// Egor_Host.FreqStripStatus.Text += "+";
}

}
}

}
catch { }
}

}
#endregion

0 Kudos
Reply

3,046 Views
ashesman
Contributor III

Thanks for that.  Is this code you have successfully used with the SDKD CDC?

0 Kudos
Reply

3,046 Views
PitOn
Contributor III
0 Kudos
Reply

3,046 Views
ashesman
Contributor III

OK.  thanks, will give it a go.  Note that the last person that posted in the forum you mention has the same problem I am having!

0 Kudos
Reply