FatFS on K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,817件の閲覧回数
hyungjunchoi
Contributor I

Hello?

I want to use FatFS on my device which has K64x MCU.

It has FreeRTOS.

Are there any Kenetis SDK components or samples for using FatFS on NXP K64x which has FreeRTOS?

Such as FatFS or internal/external Flash component?

Many Thanks,

Richard.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,658件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Hyungjun

Please refer to theusb msd fatfs demo. The application executes some FATFS APIs to test the attached device.

[SDK_2.1_FRDM-K64F]\boards\frdmk64f\usb_examples\usb_host_msd_fatfs\freertos

Hope it helps

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,658件の閲覧回数
hyungjunchoi
Contributor I

Thanks Daniel.

I'll check it.

0 件の賞賛
返信
1,659件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Hyungjun

Please refer to theusb msd fatfs demo. The application executes some FATFS APIs to test the attached device.

[SDK_2.1_FRDM-K64F]\boards\frdmk64f\usb_examples\usb_host_msd_fatfs\freertos

Hope it helps

Regards

Daniel

0 件の賞賛
返信