FatFS on K64F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FatFS on K64F

Jump to solution
1,794 Views
hyungjunchoi
Contributor I

Hello?

I want to use FatFS on my device which has K64x MCU.

It has FreeRTOS.

Are there any Kenetis SDK components or samples for using FatFS on NXP K64x which has FreeRTOS?

Such as FatFS or internal/external Flash component?

Many Thanks,

Richard.

Labels (1)
0 Kudos
Reply
1 Solution
1,635 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Hyungjun

Please refer to theusb msd fatfs demo. The application executes some FATFS APIs to test the attached device.

[SDK_2.1_FRDM-K64F]\boards\frdmk64f\usb_examples\usb_host_msd_fatfs\freertos

Hope it helps

Regards

Daniel

View solution in original post

0 Kudos
Reply
2 Replies
1,635 Views
hyungjunchoi
Contributor I

Thanks Daniel.

I'll check it.

0 Kudos
Reply
1,636 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Hyungjun

Please refer to theusb msd fatfs demo. The application executes some FATFS APIs to test the attached device.

[SDK_2.1_FRDM-K64F]\boards\frdmk64f\usb_examples\usb_host_msd_fatfs\freertos

Hope it helps

Regards

Daniel

0 Kudos
Reply