FREERTOS USB CDC HOST DEMO+FREERTOS TCP/IP ECHO DEMO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FREERTOS USB CDC HOST DEMO+FREERTOS TCP/IP ECHO DEMO

2,399件の閲覧回数
kooroshhajiani
Contributor III

I'm trying to combine the FREERTOS_TCP/IP echo Demo and FREERTOS_USB cdc host demo into one project.

I'm running into a whole host of the issues.

Has anyone been able to combine the two into one project successfully?

Regards,

Koorosh Hajiani

0 件の賞賛
返信
2 返答(返信)

1,960件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koorosh,

Can you telkl us the part number/SDK version you are using so that we can develop a project and have a try to combine them.

BR

Xiangjun rong

0 件の賞賛
返信

1,960件の閲覧回数
kooroshhajiani
Contributor III

Hi xiangjun,

Thank you for your response.

It is :

KSDK 1.3.0  and the platform is TWRK64F120.

Regards,

Koorosh Hajiani

248-778-6396

0 件の賞賛
返信