FREERTOS USB CDC HOST DEMO+FREERTOS TCP/IP ECHO DEMO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FREERTOS USB CDC HOST DEMO+FREERTOS TCP/IP ECHO DEMO

2,438 Views
kooroshhajiani
Contributor III

I'm trying to combine the FREERTOS_TCP/IP echo Demo and FREERTOS_USB cdc host demo into one project.

I'm running into a whole host of the issues.

Has anyone been able to combine the two into one project successfully?

Regards,

Koorosh Hajiani

0 Kudos
Reply
2 Replies

1,999 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koorosh,

Can you telkl us the part number/SDK version you are using so that we can develop a project and have a try to combine them.

BR

Xiangjun rong

0 Kudos
Reply

1,999 Views
kooroshhajiani
Contributor III

Hi xiangjun,

Thank you for your response.

It is :

KSDK 1.3.0  and the platform is TWRK64F120.

Regards,

Koorosh Hajiani

248-778-6396

0 Kudos
Reply