FRDM-K64f ADC and DAC Configuration in MQX RTOS based on KDS 3.0 and KDSK 1.2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K64f ADC and DAC Configuration in MQX RTOS based on KDS 3.0 and KDSK 1.2.0

1,241件の閲覧回数
homarpizar
Contributor I

Hi all,

I want to create a project using the ADC in order to read a signal created by the DAC in the same board (FRDM-K64F), but I can´t find any example whit the configuration of these to start the project.

I hope someone can help.

Best regards.

Omar.

ラベル(1)
0 件の賞賛
返信
1 返信

834件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Homar,

Please review the baremetal DAC ADC demo.  It could be implemented in a MQX application.

C:\Freescale\KSDK_1.2.0\examples\frdmk64f\demo_apps\dac_adc_demo

Documentation is in: C:\Freescale\KSDK_1.2.0\doc\Kinetis SDK v.1.2.0 Demo Applications User's Guide.pdf Chapter 7.

Regards,

David

0 件の賞賛
返信