FRDM-K64f ADC and DAC Configuration in MQX RTOS based on KDS 3.0 and KDSK 1.2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K64f ADC and DAC Configuration in MQX RTOS based on KDS 3.0 and KDSK 1.2.0

1,228 次查看
homarpizar
Contributor I

Hi all,

I want to create a project using the ADC in order to read a signal created by the DAC in the same board (FRDM-K64F), but I can´t find any example whit the configuration of these to start the project.

I hope someone can help.

Best regards.

Omar.

标签 (1)
0 项奖励
回复
1 回复

821 次查看
DavidS
NXP Employee
NXP Employee

Hi Homar,

Please review the baremetal DAC ADC demo.  It could be implemented in a MQX application.

C:\Freescale\KSDK_1.2.0\examples\frdmk64f\demo_apps\dac_adc_demo

Documentation is in: C:\Freescale\KSDK_1.2.0\doc\Kinetis SDK v.1.2.0 Demo Applications User's Guide.pdf Chapter 7.

Regards,

David

0 项奖励
回复