FRDM‑K64F‑AGM01 SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM‑K64F‑AGM01 SDK

1,301件の閲覧回数
franklay
Contributor I

Is there any SDK for FRDM‑K64F‑AGM01 running sensor fusion on the keil compiler without RTOS ?

タグ(1)
0 件の賞賛
返信
1 返信

1,188件の閲覧回数
darioarias
NXP Employee
NXP Employee

Hi Frank,

Yes, there is an SDK  with specifications you requested. You have to go to the MCUXpresso web page, and there you will be able to use the SDK builder.

  • Select the configuration FRDM-K64F-AGM01
  • Click in SDK Builder
  • Click in configurations settings
  • There you select the host OS, the IDE (Keil in this case) and deactivate FreeRTOS in optional middle ware section.
  • Finally click in request build, and download the SDK.

Inside the SDK you will find a folder in the route SDK_2.2_FRDM-K64F-AGM01 >> boards >> frdmk64f_agm01 >> issdk_examples >> algorithms>>sensorfusion with the libraries and source code.

If this didn't answer your question let me know.

Darío

0 件の賞賛
返信