Error in final launch sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in final launch sequence

2,763件の閲覧回数
rahul_eris
Contributor II

We are working on Freescale Freedom K64F Board.   IDE we are using is "Kinetis Design Studio 3.0.0" and RTOS "MQX_4_2".

Program can be build successfully.

But on flash debug(GDB open OCD Debugging), an error is occurring after about 99% of its launching .

Error shown below

 

 

 

 

Error in final launch sequence

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

localhost:3333: The system tried to join a drive to a directory on a joined drive.

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

localhost:3333: The system tried to join a drive to a directory on a joined drive.

localhost:3333: The system tried to join a drive to a directory on a joined drive.

 

 

How this problem could be solved?? ?? We are blocked with this and delayed in our development activity.

Hoping for a solution asap.

 

 

 

Thanks,

Rahul

ERIS Labs PVT LTD

 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,838件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Same question has been asked here:Error in final launch sequence

0 件の賞賛
返信