Does KSDK support K60F120M device ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does KSDK support K60F120M device ?

ソリューションへジャンプ
4,926件の閲覧回数
davidchen-b3693
NXP Employee
NXP Employee

Hi Sir :

     I not find K60F120M in KSDK support list . Does that mean KSDK not support K60F120M device ?

Thanks .

 

Best regards,

David

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,522件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello David,

Yes, exactly. K60F120M is not supported right now and actually I don´t see support in plan for KSDK 1.3

All supported MCU you see in Release Note or some information are also at ARM Cortex-M4 Cores|Kinetis K MCUs|Freescale

productselector.png

For other cases (unsupported/custom chip), you can modify it according to yourself.

I´m attaching the guide.

I hope it helps you.

Best Regards,

Iva

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,523件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello David,

Yes, exactly. K60F120M is not supported right now and actually I don´t see support in plan for KSDK 1.3

All supported MCU you see in Release Note or some information are also at ARM Cortex-M4 Cores|Kinetis K MCUs|Freescale

productselector.png

For other cases (unsupported/custom chip), you can modify it according to yourself.

I´m attaching the guide.

I hope it helps you.

Best Regards,

Iva

0 件の賞賛
返信
4,522件の閲覧回数
davidchen-b3693
NXP Employee
NXP Employee

Hi Iva :

     Much thanks for your information .

Best regards,

David

0 件の賞賛
返信
4,522件の閲覧回数
sohalpatel
Contributor II

Hello David,

I'd be interested to port lwip to the K60F120 tower board. It seems we share the same problem. Have you been successful in migrating?

Thanks and Merry Christmas

Sohal.

0 件の賞賛
返信
4,522件の閲覧回数
davidchen-b3693
NXP Employee
NXP Employee

Hi Sohal :

     Merry Christmas !!

Finally , we did not migrate the SDK to K60F120M .

There is a sharing that I did before to migrate K64 to KL26 . KL26 is also not listed in KSDK 1.1.0 . I  hope that helpful .

KSDK-Migrate project to a new device 

Best regards,

David

0 件の賞賛
返信