Disable RESET_PIN on MKL03Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable RESET_PIN on MKL03Z

2,054 Views
renejespersen
Contributor I


Hello.
I am pretty much stucked here. I want to disable the RESET_PIN on my MKL03Z as i want to use it as GPIO.

 

I do not have access to Processor Expert in my project, so i need to do this the "hard" way. In the documentation it is stated that i can disable it by setting RESET_PIN_CFG option bit to 0. But I can't figure out how to do this using the Kinetis SDK.

According to this document it is a part of the NV_FOPT field. But I can't find a way to configure this in the SDK.
https://community.nxp.com/servlet/JiveServlet/download/457218-1-283909/Reset_pin_redefinition.pdf

 

Please help me figure this out. I am a bit lost

 

Best regards.

Rene Jespersen

Labels (1)
0 Kudos
Reply
2 Replies

1,846 Views
DavidS
NXP Employee
NXP Employee

Hi Rene,

Below is my configuration to disable the RESET pin:

/* Flash Configuration */

    .section .FlashConfig, "a"

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFF35FE /* //DES was 0xFFFF3DFE ...disable RESET pin */

Regards,

David

0 Kudos
Reply

1,846 Views
renejespersen
Contributor I

I have tried to edit the Flash Configuration in startup_MKL03Z4.s. The reset button still works. From section 6.3.2 FOPT boot options in the documentation the RESET_PIN_CFG is on bit number 3. As I can figure out it FOPT should be at 0x040D and if i set it to disable RESET_PIN_CFG and boot from flash i get 00110111 = 0x37 which i put on 0x040D as below. Now it works :smileyhappy:

/* Flash Configuration */

    .section .FlashConfig, "a"

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFF37FE

    .text

    .thumb

0 Kudos
Reply