Compiling the KDSK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiling the KDSK

2,649件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I am trying to build the lbrary. I get incomprehensible problems building with the command line and I prefer to build using the CodeWarrior framework.

I will need the ethernet, and in the path boards\common I find two directories : phyksz8041 and phyksz8081. They appear to be mutually exclusive.

Which one to choice?

 

 

Thank You

 

Pietro

ラベル(1)
タグ(3)
3 返答(返信)

2,443件の閲覧回数
pietrodicastri
Senior Contributor II

Hi Jorge

The final target will follow the one on the FRDM platform. I see the names ksz8041 and ksz8081 follow the names of the micrel devices which should be used

for using the example codes as they are. Confirm me this consideration please.

I have compiled the KDSK with the CodeWarrior using some force, I did not test but I am confident.

I wait for Your reply

Thank You

0 件の賞賛
返信

2,443件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Pietro:

That is correct, the folders are named according to the phy device.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,443件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Pietro di Castri:

KSDK is only available right now for a few boards, what device do you have?

Also KSDK is not prepared to be compiled with CodeWarrior since CW will not be supported. You can use instead KDS, IAR, Keil or GCC standalone tools.

Regarding the directories, the correct folder depends again on the board you use. e.g. in the TWR-SER board used with the different MCU tower boards, there is a ksz8041 Ethernet phy, while the FRDM-K64F has a ksz8081.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信