Changing MCU target used on driver example projects

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Changing MCU target used on driver example projects

跳至解决方案
1,461 次查看
jschoen
Contributor III

Using one of the driver examples for FRDM-KL03 (e.g. adc16).  KSDK1.3 and KDS 3.0.

 

What needs to be changed to target 8K Flash version of the KL03 instead of the 32K version?  Is it just the linker file?

标签 (1)
0 项奖励
回复
1 解答
1,364 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Because the chip is the same, just flash or RAM size are different, so i think it is okay for you just to update the linker file, chnange memory address and length in linker file.

Hope it can help you.

BR

Xiangjun Rong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,365 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Because the chip is the same, just flash or RAM size are different, so i think it is okay for you just to update the linker file, chnange memory address and length in linker file.

Hope it can help you.

BR

Xiangjun Rong

0 项奖励
回复