Changing MCU target used on driver example projects

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing MCU target used on driver example projects

ソリューションへジャンプ
1,450件の閲覧回数
jschoen
Contributor III

Using one of the driver examples for FRDM-KL03 (e.g. adc16).  KSDK1.3 and KDS 3.0.

 

What needs to be changed to target 8K Flash version of the KL03 instead of the 32K version?  Is it just the linker file?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,353件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Because the chip is the same, just flash or RAM size are different, so i think it is okay for you just to update the linker file, chnange memory address and length in linker file.

Hope it can help you.

BR

Xiangjun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,354件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Because the chip is the same, just flash or RAM size are different, so i think it is okay for you just to update the linker file, chnange memory address and length in linker file.

Hope it can help you.

BR

Xiangjun Rong

0 件の賞賛
返信