Abnormal output port signal triggered by printf()

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Abnormal output port signal triggered by printf()

1,714 次查看
petershih
Contributor III

Hi:

 

I am working on a custom board equipped with K66 MCU(120MHz, and 60MHz bus clock) and other peripherals. Recently, I am facing a issue regarding printf(). I have PTC13 as input port, and PTC3 and PTC4 from UART1 as debug port for my project. I discovered whenever the printf() output words, the PTC13 also change status. For diagnostic purpose, I set the PTE0 port before printf(), and clear the port after printf(). Based on the scope, I can pretty sure the strange PTC3 outputs are from printf(). As I mentioned the PTC13 is declare as input (verified by PCR13_MUX=1), I have no idea how this port can be toggled as output. Please help me out if you have any idea or recommendation. Thank you very much.

 

Yellow signal: PTC13 (GPIO input),

Red signal: PTE0 (GPIO output) for diagnostic purpose only.

115366_115366.pngpastedImage_0.png

115970_115970.pngpastedImage_21.png

In Main.c:

int main(void) {     /* Write your code here */     // Init hardware     hardware_init();     gpio_Init();      GPIOE_PSOR |= 0x00000001;     PRINTF("\r\n Test Start:\r\n");     GPIOE_PCOR |= 0x00000001;      /* This for loop should be replaced. By default this loop allows a single stepping. */     for (;;) {         i++;         if (!i)    {             GPIOE_PSOR |= 0x00000001;             PRINTF(".");             GPIOE_PCOR |= 0x00000001;         }     }     /* Never leave main */     return 0; }  void gpio_Init(void) {     gpio_input_pin_user_config_t     inputPinConfig;     gpio_output_pin_user_config_t     outputPinConfig;      outputPinConfig.pinName = kGpioE0;     outputPinConfig.config.outputLogic = 0;     outputPinConfig.config.slewRate = kPortSlowSlewRate;     outputPinConfig.config.isOpenDrainEnabled = false;     outputPinConfig.config.driveStrength = kPortLowDriveStrength;     GPIO_DRV_OutputPinInit(&outputPinConfig);      inputPinConfig.pinName = kGpioC13;     inputPinConfig.config.isPullEnable = false;     inputPinConfig.config.pullSelect = kPortPullUp;     inputPinConfig.config.isPassiveFilterEnabled = false;     inputPinConfig.config.isDigitalFilterEnabled = false;     inputPinConfig.config.interrupt = kPortIntDisabled;     GPIO_DRV_InputPinInit(&inputPinConfig); }

 

In pin_mux.c:

void configure_uart_pins(uint32_t instance) {   switch(instance) {     case UART1_IDX:       /* Affects PORTE_PCR17 register */       PORT_HAL_SetMuxMode(PORTC,3UL,kPortMuxAlt3);       /* Affects PORTE_PCR16 register */       PORT_HAL_SetMuxMode(PORTC,4UL,kPortMuxAlt3);       break;     case UART2_IDX:                      /* HW_UART2 */       /* Affects PORTD_PCR2 register */       PORT_HAL_SetMuxMode(PORTD,2UL,kPortMuxAlt3);       /* Affects PORTD_PCR3 register */       PORT_HAL_SetMuxMode(PORTD,3UL,kPortMuxAlt3);       break;     case UART4_IDX:                      /* HW_UART4 */       /* Affects PORTC_PCR14 register */       PORT_HAL_SetMuxMode(PORTC,14UL,kPortMuxAlt3);       /* Affects PORTC_PCR15 register */       PORT_HAL_SetMuxMode(PORTC,15UL,kPortMuxAlt3);       break;     default:       break;   } }

 

In hardware_init.c

void hardware_init(void) {     /* enable clock for PORTs */     CLOCK_SYS_EnablePortClock(PORTA_IDX);     CLOCK_SYS_EnablePortClock(PORTB_IDX);     CLOCK_SYS_EnablePortClock(PORTC_IDX);     CLOCK_SYS_EnablePortClock(PORTD_IDX);     CLOCK_SYS_EnablePortClock(PORTE_IDX);      /* Init board clock */     BOARD_ClockInit();     dbg_uart_init();      /* Set clock source for Ethernet */ //    if (0 == strcmp("TWR-K65F180M", BOARD_NAME)) //    { //        CLOCK_SYS_SetEnetRmiiSrc(ENET_IDX, kClockRmiiSrcExt); //    } }

 

In board.c

/* Initialize debug console. */ void dbg_uart_init(void) {     configure_uart_pins(BOARD_DEBUG_UART_INSTANCE);      DbgConsole_Init(BOARD_DEBUG_UART_INSTANCE, BOARD_DEBUG_UART_BAUD, kDebugConsoleUART); }

 

Peter Shih

标签 (1)
标记 (3)
0 项奖励
回复
4 回复数

1,337 次查看
petershih
Contributor III

Hi:

I have tried to printf() to different port, for example UART4 on PTC14 and 15. It doesn't have any problem. I don't see any abnormal signal on PTC13.

I also tried to output debug message by  UART_DRV_SendData() instead of printf(). I still see the abnormal signal from PTC13. It looks like the PTC13 has some kind of relationship with UART1. Any idea? please let me know. Thanks!

static uint16_t i = 0;

static uint8_t msg1[]="\r\n Test Start:\r\n";

uart_state_t        uart1State;

int main(void)

{

    /* Write your code here */

    // Init hardware

    hardware_init();

    uart1_init();

    gpio_Init();

    GPIOE_PSOR |= 0x00000001;

    //PRINTF("\r\n Test Start:\r\n");

    UART_DRV_SendData(BOARD_DEBUG_UART_INSTANCE, msg1, sizeof(msg1));

    while (kStatus_UART_TxBusy == UART_DRV_GetTransmitStatus(BOARD_DEBUG_UART_INSTANCE, NULL)){}

    GPIOE_PCOR |= 0x00000001;

    /* This for loop should be replaced. By default this loop allows a single stepping. */

    for (;;) {

        i++;

        if (!i)    {

            GPIOE_PSOR |= 0x00000001;

            //PRINTF(".");

            UART_DRV_SendData(BOARD_DEBUG_UART_INSTANCE, ".", 1);

            while (kStatus_UART_TxBusy == UART_DRV_GetTransmitStatus(BOARD_DEBUG_UART_INSTANCE, NULL)){}

            GPIOE_PCOR |= 0x00000001;

        }

    }

    /* Never leave main */

    return 0;

}

void uart1_init(void)

{

    uart_user_config_t     uartConfig;

    configure_uart_pins(BOARD_DEBUG_UART_INSTANCE);

    uartConfig.bitCountPerChar = kUart8BitsPerChar;

    uartConfig.parityMode      = kUartParityDisabled;

    uartConfig.stopBitCount    = kUartOneStopBit;

    uartConfig.baudRate        = BOARD_DEBUG_UART_BAUD;

    // Initialize the uart module with base address and config structure

    UART_DRV_Init(BOARD_DEBUG_UART_INSTANCE, &uart1State, &uartConfig);

}

void UART1_RX_TX_IRQHandler(void)

{

    UART_DRV_IRQHandler(1);

}

0 项奖励
回复

1,336 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  

0 项奖励
回复

1,337 次查看
petershih
Contributor III

Hi Alice:

The UART1 transfer data correctly. I am able to see the correct message sent through UART1 on PC with Tera Term software.

Whenever UART1 transfer data, I can see PTC13 status changed also. This is weird since the PTC13 is declare as input pin, and this port is nothing to do with UART1. As I mentioned this is on a custom board with K66 MCU. I am also sending you the project file for your review. the project is sending "." character constantly through UART1 at 115200 baud. The following are the signal captures by scope.

yellow signal: UART1_TX, sending '.' every 5ms.

red signal: PTC13 signal.

pastedImage_0.png

pastedImage_1.png

Please let me know if you have any idea. Thanks!

0 项奖励
回复

1,337 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  peter,

Please configure the internal pullup or pulldown for the PTC13, that is to say change the "false" to "true"

pastedImage_0.png

or it will the electrical disturebance on your board .

Hope it helps

Alice

0 项奖励
回复