Hello community,
This document is the continuation of the documents Line scan camera with KSDK [ADC + PIT + GPIO] and Controlling speed in DC motors and position in servomotors with KSDK [FTM + GPIO] which show the ease of use of the peripheral drivers from Kinetis SDK applied to the Freescale Cup smart car. This time I bring to you a document which explains an easy way to detect the track's line from the data acquired with the linear camera.
The required material to run this project is:
- A Servomotor (the project supports up to two servomotors, one servomotor is included in the smart car kit).
- Two DC motors (included in the smart car kit).
- Line scan camera (the project supports up to two cameras).
- FRDM-KL25Z based on the Kinetis Microcontroller KL25Z.
- FRDM-TFC shield.
- Mini-USB cable.
This material can be bought in The Freescale Cup Intelligent Car Development.



If you are interested in participate in the Freescale Cup you could take a look into the groups University Programs, TFC - Mexico, TFC - Brazil, TFC - China, TFC - Malaysia, TFC - Japan, TFC - North America, TFC - India, TFC - Taiwan, The Freescale Cup EMEA.
Best regards,
Earl Orlando Ramírez-Sánchez
Technical Support Engineer
Freescale Semiconductor